ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line
733
of file
em_acmp.h
.
#include <
em_acmp.h
>
Data Fields |
|
| ACMP_Accuracy_TypeDef | accuracy |
| uint32_t | biasProg |
| bool | enable |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
| bool | inactiveValue |
| ACMP_InputRange_TypeDef | inputRange |
| uint32_t | vrefDiv |
Field Documentation
| ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
Definition at line
771
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line
748
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line
823
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
| bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
Definition at line
804
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range. Adjust this setting to optimize the performance for a given input voltage range.
Definition at line
763
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| uint32_t ACMP_Init_TypeDef::vrefDiv |
VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
Definition at line
815
of file
em_acmp.h
.
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_acmp.h