AMUXCP_TypeDef Struct ReferenceDevices > AMUXCP
AMUXCP Register Declaration.
Definition at line
48
of file
efr32mg21_amuxcp.h
.
#include <
efr32mg21_amuxcp.h
>
Data Fields |
|
| __IOM uint32_t | CTRL |
| __IOM uint32_t | CTRL_CLR |
| __IOM uint32_t | CTRL_SET |
| __IOM uint32_t | CTRL_TGL |
| __IM uint32_t | IPVERSION |
| __IM uint32_t | IPVERSION_CLR |
| __IM uint32_t | IPVERSION_SET |
| __IM uint32_t | IPVERSION_TGL |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1018U] |
| uint32_t | RESERVED2 [1U] |
| uint32_t | RESERVED3 [1018U] |
| uint32_t | RESERVED4 [1U] |
| uint32_t | RESERVED5 [1018U] |
| uint32_t | RESERVED6 [1U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | STATUS_CLR |
| __IM uint32_t | STATUS_SET |
| __IM uint32_t | STATUS_TGL |
| __IOM uint32_t | TEST |
| __IOM uint32_t | TEST_CLR |
| __IOM uint32_t | TEST_SET |
| __IOM uint32_t | TEST_TGL |
| __IOM uint32_t | TRIM |
| __IOM uint32_t | TRIM_CLR |
| __IOM uint32_t | TRIM_SET |
| __IOM uint32_t | TRIM_TGL |
Field Documentation
| __IOM uint32_t AMUXCP_TypeDef::CTRL |
Control
Definition at line
51
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::CTRL_CLR |
Control
Definition at line
65
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::CTRL_SET |
Control
Definition at line
58
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::CTRL_TGL |
Control
Definition at line
72
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::IPVERSION |
IPVERSION
Definition at line
49
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::IPVERSION_CLR |
IPVERSION
Definition at line
63
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::IPVERSION_SET |
IPVERSION
Definition at line
56
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::IPVERSION_TGL |
IPVERSION
Definition at line
70
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED1[1018U] |
Reserved for future use
Definition at line
55
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line
57
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED3[1018U] |
Reserved for future use
Definition at line
62
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED4[1U] |
Reserved for future use
Definition at line
64
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED5[1018U] |
Reserved for future use
Definition at line
69
of file
efr32mg21_amuxcp.h
.
| uint32_t AMUXCP_TypeDef::RESERVED6[1U] |
Reserved for future use
Definition at line
71
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::STATUS |
Status
Definition at line
52
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::STATUS_CLR |
Status
Definition at line
66
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::STATUS_SET |
Status
Definition at line
59
of file
efr32mg21_amuxcp.h
.
| __IM uint32_t AMUXCP_TypeDef::STATUS_TGL |
Status
Definition at line
73
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TEST |
Test
Definition at line
53
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TEST_CLR |
Test
Definition at line
67
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TEST_SET |
Test
Definition at line
60
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TEST_TGL |
Test
Definition at line
74
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TRIM |
New Register
Definition at line
54
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TRIM_CLR |
New Register
Definition at line
68
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TRIM_SET |
New Register
Definition at line
61
of file
efr32mg21_amuxcp.h
.
| __IOM uint32_t AMUXCP_TypeDef::TRIM_TGL |
New Register
Definition at line
75
of file
efr32mg21_amuxcp.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_amuxcp.h