IADC_InitSingle_t Struct ReferenceEMLIB > IADC
IADC single init structure
Definition at line
722
of file
em_iadc.h
.
#include <
em_iadc.h
>
Data Fields |
|
| IADC_Alignment_t | alignment |
| uint8_t | dataValidLevel |
| bool | fifoDmaWakeup |
| bool | showId |
| bool | singleTailgate |
| bool | start |
| IADC_TriggerAction_t | triggerAction |
| IADC_TriggerSel_t | triggerSelect |
Field Documentation
| IADC_Alignment_t IADC_InitSingle_t::alignment |
Alignment of data in FIFO.
Definition at line
723
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| uint8_t IADC_InitSingle_t::dataValidLevel |
Data valid level before requesting DMA transfer.
Definition at line
725
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| bool IADC_InitSingle_t::fifoDmaWakeup |
Wake-up DMA when FIFO reaches data valid level.
Definition at line
726
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| bool IADC_InitSingle_t::showId |
Tag FIFO entry with single indicator (0x20).
Definition at line
724
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| bool IADC_InitSingle_t::singleTailgate |
If true, wait until end of SCAN queue before single queue warmup and conversion.
Definition at line
729
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| bool IADC_InitSingle_t::start |
Start scan immediately.
Definition at line
731
of file
em_iadc.h
.
Referenced by IADC_initSingle() .
| IADC_TriggerAction_t IADC_InitSingle_t::triggerAction |
| IADC_TriggerSel_t IADC_InitSingle_t::triggerSelect |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_iadc.h