MSCEMLIB
Detailed Description
Memory System Controller API.
Contains functions to control the MSC, primarily the Flash. Users can perform Flash memory write and erase operations, as well as optimization of the CPU instruction fetch interface for the application. Available instruction fetch features depends on the MCU or SoC family, but features such as instruction pre-fetch, cache, and configurable branch prediction are typically available.
- Note
 - Flash wait-state configuration is handled by CMU module. When core clock configuration is changed by a call to functions such as CMU_ClockSelectSet() or CMU_HFRCOBandSet(), then Flash wait-state configuration is also updated.
 
MSC resets into a safe state. To initialize the instruction interface to recommended settings:
- Note
 - The optimal configuration is highly application dependent. Performance benchmarking is supported by most families. See MSC_StartCacheMeasurement() and MSC_GetCacheMeasurement() for more details.
 
Support for Flash write and erase runs from RAM by default. This code may be allocated to Flash by defining EM_MSC_RUN_FROM_FLASH .
- Note
 - Flash erase may add ms of delay to interrupt latency if executing from Flash.
 
Flash write and erase operations are supported by MSC_WriteWord() , MSC_WriteWordFast(), MSC_ErasePage() , and MSC_MassErase(). Fast write is not supported for EFM32G and mass erase is supported for MCU and SoC families with larger Flash sizes.
- Note
 - MSC_Init() must be called prior to any Flash write or erase operation.
 
The following steps are necessary to perform a page erase and write:
         Data Structures | 
       |
| struct | MSC_EccConfig_TypeDef | 
| struct | MSC_ExecConfig_TypeDef | 
         Macros | 
       |
| #define | EM_MSC_RUN_FROM_FLASH | 
| 
         By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
          | 
       |
| #define | MSC_ECC_BANKS (1) | 
| #define | MSC_ECCCONFIG_DEFAULT | 
| #define | MSC_EXECCONFIG_DEFAULT | 
| #define | MSC_PROGRAM_TIMEOUT 10000000ul | 
| 
         Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
          | 
       |
| #define | MSC_RAMFUNC_DECLARATOR | 
| 
         Expands to
         
          SL_RAMFUNC_DECLARATOR
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
| #define | MSC_RAMFUNC_DEFINITION_BEGIN | 
| 
         Expands to
         
          SL_RAMFUNC_DEFINITION_BEGIN
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
| #define | MSC_RAMFUNC_DEFINITION_END | 
| 
         Expands to
         
          SL_RAMFUNC_DEFINITION_END
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
         Enumerations | 
       |
| enum | 
         
          MSC_Status_TypeDef
         
         {
          mscReturnOk = 0, mscReturnInvalidAddr = -1, mscReturnLocked = -2, mscReturnTimeOut = -3, mscReturnUnaligned = -4 }  | 
       
         Functions | 
       |
| void | MSC_Deinit (void) | 
| 
         Turn off MSC flash write enable and lock MSC registers.
          | 
       |
| void | MSC_EccConfigSet ( MSC_EccConfig_TypeDef *eccConfig) | 
| 
         Configure Error Correcting Code (ECC)
          | 
       |
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_ErasePage (uint32_t *startAddress) | 
| 
         Erases a page in flash memory.
          | 
       |
| void | MSC_ExecConfigSet ( MSC_ExecConfig_TypeDef *execConfig) | 
| 
         Set MSC code execution configuration.
          | 
       |
| void | MSC_Init (void) | 
| 
         Initialize MSC module. Puts MSC hw in a known state.
          | 
       |
| __STATIC_INLINE void | MSC_IntClear (uint32_t flags) | 
| 
         Clear one or more pending MSC interrupts.
          | 
       |
| __STATIC_INLINE void | MSC_IntDisable (uint32_t flags) | 
| 
         Disable one or more MSC interrupts.
          | 
       |
| __STATIC_INLINE void | MSC_IntEnable (uint32_t flags) | 
| 
         Enable one or more MSC interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | MSC_IntGet (void) | 
| 
         Get pending MSC interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | MSC_IntGetEnabled (void) | 
| 
         Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
          | 
       |
| __STATIC_INLINE void | MSC_IntSet (uint32_t flags) | 
| 
         Set one or more pending MSC interrupts from SW.
          | 
       |
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWord (uint32_t *address, void const *data, uint32_t numBytes) | 
| 
         Writes data to flash memory. Write data must be aligned to words and contain a number of bytes that is divisable by four.
          | 
       |
| static void | mscEccBankDisable (const MSC_EccBank_Typedef *eccBank) | 
| 
         Disable ECC for a given memory bank.
          | 
       |
| static void | mscEccBankInit (const MSC_EccBank_Typedef *eccBank, uint32_t dmaChannels[2]) | 
| 
         Initialize ECC for a given memory bank.
          | 
       |
| static MSC_RAMFUNC_DEFINITION_END void | mscEccReadWriteExistingDma (uint32_t start, uint32_t size, uint32_t channels[2]) | 
| 
         DMA read and write existing values (for ECC initializaion).
          | 
       |
Macro Definition Documentation
| #define EM_MSC_RUN_FROM_FLASH | 
By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
- Note
 - This define is not present by default. The MSC controller API will run from RAM by default.
 
        Definition at line
        
         124
        
        of file
        
         em_msc.h
        
        .
       
| #define MSC_ECC_BANKS (1) | 
EFR32XG21 incorporates 1 memory bank including ECC support.
        Definition at line
        
         211
        
        of file
        
         em_msc.h
        
        .
       
Referenced by MSC_EccConfigSet() .
| #define MSC_ECCCONFIG_DEFAULT | 
Default MSC EccConfig initialization
        Definition at line
        
         213
        
        of file
        
         em_msc.h
        
        .
       
| #define MSC_EXECCONFIG_DEFAULT | 
Default MSC ExecConfig initialization
        Definition at line
        
         157
        
        of file
        
         em_msc.h
        
        .
       
| #define MSC_PROGRAM_TIMEOUT 10000000ul | 
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
- Note
 - Timeout is set very large (in the order of 100x longer than necessary). This is to avoid any corner case.
 
        Definition at line
        
         109
        
        of file
        
         em_msc.h
        
        .
       
Enumeration Type Documentation
| enum MSC_Status_TypeDef | 
Return codes for writing/erasing Flash.
        Definition at line
        
         132
        
        of file
        
         em_msc.h
        
        .
       
Function Documentation
| void MSC_EccConfigSet | ( | MSC_EccConfig_TypeDef * | 
           
            eccConfig
           
           | 
          ) | 
Configure Error Correcting Code (ECC)
This function configures ECC support according to the configuration input parameter. If the user requests enabling ECC for a given RAM bank this function will initialize ECC memory (syndromes) for the bank by reading and writing the existing values in memory. I.e. all data is preserved. The initialization process runs in a critical section disallowing interrupts and thread scheduling, and will consume a considerable amount of clock cycles. Therefore the user should carefully assess where to call this function. The user can consider to increase the clock frequency in order to reduce the execution time. This function makes use of 2 DMA channels to move data to/from RAM in an efficient way. The user can select which 2 DMA channels to use in order to avoid conflicts with the application. However the user must make sure that no other DMA operations takes place while this function is executing. If the application has been using the DMA controller prior to calling this function, the application will need to reinitialize DMA registers after this function has completed.
- Note
 - 
         This function protects the ECC initialization procedure from interrupts and other threads by using a critical section (defined by
         
em_core.h) When running on RTOS the user may need to override CORE_EnterCritical CORE_ExitCritical which are declared as 'SL_WEAK' in em_core.c . 
- Parameters
 - 
         
[in] eccConfigECC configuration  
        Definition at line
        
         1565
        
        of file
        
         em_msc.c
        
        .
       
References MSC_EccConfig_TypeDef::dmaChannels , MSC_EccConfig_TypeDef::enableEccBank , MSC , MSC_ECC_BANKS , mscEccBankDisable() , and mscEccBankInit() .
| MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_ErasePage | ( | uint32_t * | 
           
            startAddress
           
           | 
          ) | 
Erases a page in flash memory.
- Note
 - It is recommended to run this code from RAM.
 
For IAR, Rowley, SimplicityStudio, Atollic and armgcc this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
 - 
         
[in] startAddressPointer to the flash page to erase. Must be aligned to beginning of page boundary.  
- Returns
 - 
         Returns the status of erase operation,
         
          MSC_Status_TypeDef
         
         
* mscReturnOk - Operation completed successfully. * mscReturnInvalidAddr - Operation tried to erase a non-flash area. * flashReturnLocked - MSC registers are locked or the operation tried to * erase a locked area of the flash. * flashReturnTimeOut - Operation timed out. *
 
        Definition at line
        
         457
        
        of file
        
         em_msc.c
        
        .
       
References FLASH_PAGE_SIZE , MSC , MSC_LOCK_LOCKKEY_LOCK , MSC_LOCK_LOCKKEY_UNLOCK , MSC_STATUS_BUSY , MSC_WRITECMD_ERASEPAGE , and MSC_WRITECTRL_WREN .
Referenced by NVMHAL_PageErase() .
| void MSC_ExecConfigSet | ( | MSC_ExecConfig_TypeDef * | 
           
            execConfig
           
           | 
          ) | 
Set MSC code execution configuration.
- Parameters
 - 
         
[in] execConfigCode execution configuration  
        Definition at line
        
         419
        
        of file
        
         em_msc.c
        
        .
       
References MSC_ExecConfig_TypeDef::doutBufEn , MSC , and MSC_READCTRL_DOUTBUFEN .
| __STATIC_INLINE void MSC_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending MSC interrupts.
- Parameters
 - 
         
[in] flagsPending MSC intterupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         248
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more MSC interrupts.
- Parameters
 - 
         
[in] flagsMSC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         265
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more MSC interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using MSC_IntClear() prior to enabling the interrupt.
 
- Parameters
 - 
         
[in] flagsMSC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         287
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending MSC interrupt flags.
- Note
 - The event bits are not cleared by the use of this function.
 
- Returns
 - MSC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
 
        Definition at line
        
         307
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Interrupt flags are not cleared by the use of this function.
 
- Returns
 - 
         Pending and enabled MSC interrupt sources. The return value is the bitwise AND of
         
- the enabled interrupt sources in MSC_IEN and
 - the pending interrupt flags MSC_IF
 
 
        Definition at line
        
         326
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending MSC interrupts from SW.
- Parameters
 - 
         
[in] flagsMSC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         342
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWord | ( | uint32_t * | 
           
            address,
           
           | 
         
| void const * | 
           
            data,
           
           | 
         ||
| uint32_t | 
           
            numBytes
           
           | 
         ||
| ) | 
Writes data to flash memory. Write data must be aligned to words and contain a number of bytes that is divisable by four.
- Note
 - It is recommended to erase the flash page before performing a write.
 
It is recommended to run this code from RAM.
For IAR, Rowley, SimplicityStudio, Atollic and armgcc this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
 - 
         
[in] addressPointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesNumber of bytes to write to flash. NB: Must be divisable by four.  
- Returns
 - 
         Returns the status of the write operation,
         
          MSC_Status_TypeDef
         
         
* flashReturnOk - Operation completed successfully. * flashReturnInvalidAddr - Operation tried to write to a non-flash area. * flashReturnLocked - MSC registers are locked or the operation tried to * program a locked area of the flash. * flashReturnTimeOut - Operation timed out. *
 
        Definition at line
        
         513
        
        of file
        
         em_msc.c
        
        .
       
References FLASH_PAGE_SIZE , MSC , MSC_LOCK_LOCKKEY_LOCK , MSC_LOCK_LOCKKEY_UNLOCK , MSC_WRITECTRL_WREN , mscReturnOk , and SL_MIN .
Referenced by DBG_DisableDebugAccess() , and NVMHAL_Write() .
           
  | 
          static | 
Disable ECC for a given memory bank.
This function disables ECC for a given memory bank which is specified with the MSC_EccBank_Typedef structure input parameter.
- Parameters
 - 
         
[in] eccBankECC memory bank device structure.  
        Definition at line
        
         1528
        
        of file
        
         em_msc.c
        
        .
       
Referenced by MSC_EccConfigSet() .
           
  | 
          static | 
Initialize ECC for a given memory bank.
This function initializes ECC for a given memory bank which is specified with the MSC_EccBank_Typedef structure input parameter.
- Parameters
 - 
         
[in] eccBankECC memory bank device structure. [in] dmaChannelsArray of 2 DMA channels that may be used during ECC initialization.  
        Definition at line
        
         1487
        
        of file
        
         em_msc.c
        
        .
       
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_CRITICAL , CORE_EXIT_CRITICAL , and mscEccReadWriteExistingDma() .
Referenced by MSC_EccConfigSet() .
           
  | 
          static | 
DMA read and write existing values (for ECC initializaion).
This function uses DMA to read and write the existing data values in the RAM region specified by start and size. The function will use the 2 DMA channels specified by the channels[2] array.
- Parameters
 - 
         
[in] startStart address of address range in RAM to read/write. [in] sizeSize of address range in RAM to read/write. [in] channels[2]Array of 2 DMA channels to use.  
        Definition at line
        
         1374
        
        of file
        
         em_msc.c
        
        .
       
References _LDMA_CH_CTRL_XFERCNT_MASK , _LDMA_CH_LINK_LINKADDR_MASK , _LDMA_CTRL_NUMFIXED_SHIFT , BUS_RegMaskedClear() , CMU_ClockEnable() , cmuClock_LDMA , LDMA , LDMA_CH_CTRL_BLOCKSIZE_ALL , LDMA_CH_CTRL_DSTINC_ONE , LDMA_CH_CTRL_REQMODE_ALL , LDMA_CH_CTRL_SIZE_WORD , LDMA_CH_CTRL_SRCINC_ONE , LDMA_CH_CTRL_STRUCTREQ , LDMA_CH_CTRL_STRUCTTYPE_TRANSFER , LDMA_CH_LINK_LINK , and LDMA_EN_EN .
Referenced by mscEccBankInit() .