GPIO_LETIMERROUTE_TypeDef Struct ReferenceDevices
Definition at line
74
of file
efr32mg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | OUT0ROUTE |
| __IOM uint32_t | OUT1ROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_LETIMERROUTE_TypeDef::OUT0ROUTE |
OUT0 port/pin select
Definition at line
76
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_LETIMERROUTE_TypeDef::OUT1ROUTE |
OUT1 port/pin select
Definition at line
77
of file
efr32mg21_gpio.h
.
| uint32_t GPIO_LETIMERROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
78
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_LETIMERROUTE_TypeDef::ROUTEEN |
LETIMER pin enable
Definition at line
75
of file
efr32mg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_gpio.h