TIMER_CC_TypeDef Struct ReferenceDevices > TIMER
TIMER CC Register Group Declaration.
Definition at line
48
of file
efr32mg21_timer.h
.
#include <
efr32mg21_timer.h
>
Data Fields |
|
| __IOM uint32_t | CFG |
| __IOM uint32_t | CTRL |
| __IM uint32_t | ICF |
| __IM uint32_t | ICOF |
| __IOM uint32_t | OC |
| __IOM uint32_t | OCB |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1U] |
Field Documentation
| __IOM uint32_t TIMER_CC_TypeDef::CFG |
CC Channel Configuration Register
Definition at line
49
of file
efr32mg21_timer.h
.
Referenced by TIMER_CaptureBufGet() , TIMER_CaptureGet() , TIMER_InitCC() , and TIMER_Reset() .
| __IOM uint32_t TIMER_CC_TypeDef::CTRL |
CC Channel Control Register
Definition at line
50
of file
efr32mg21_timer.h
.
Referenced by TIMER_InitCC() , and TIMER_Reset() .
| __IM uint32_t TIMER_CC_TypeDef::ICF |
IC Channel Value Register
Definition at line
54
of file
efr32mg21_timer.h
.
Referenced by TIMER_CaptureGet() .
| __IM uint32_t TIMER_CC_TypeDef::ICOF |
IC Channel Value Overflow Register
Definition at line
55
of file
efr32mg21_timer.h
.
Referenced by TIMER_CaptureBufGet() .
| __IOM uint32_t TIMER_CC_TypeDef::OC |
OC Channel Value Register
Definition at line
51
of file
efr32mg21_timer.h
.
Referenced by TIMER_CaptureGet() , TIMER_CompareSet() , and TIMER_Reset() .
| __IOM uint32_t TIMER_CC_TypeDef::OCB |
OC Channel Value Buffer Register
Definition at line
53
of file
efr32mg21_timer.h
.
Referenced by TIMER_CaptureBufGet() , TIMER_CompareBufSet() , and TIMER_Reset() .
| uint32_t TIMER_CC_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
52
of file
efr32mg21_timer.h
.
| uint32_t TIMER_CC_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
56
of file
efr32mg21_timer.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_timer.h