CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU
LFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
       Definition at line
       
        289
       
       of file
       
        em_cmu.h
       
       .
      
      
       #include <
       
     
        em_cmu.h
       
       >
      
         Data Fields | 
       |
| bool | agcEn | 
| uint8_t | capTune | 
| bool | disOnDemand | 
| bool | failDetEM4WUEn | 
| bool | failDetEn | 
| bool | forceEn | 
| uint8_t | gain | 
| bool | highAmplitudeEn | 
| CMU_LfxoOscMode_TypeDef | mode | 
| bool | regLock | 
| CMU_LfxoStartupDelay_TypeDef | timeout | 
Field Documentation
| bool CMU_LFXOInit_TypeDef::agcEn | 
| uint8_t CMU_LFXOInit_TypeDef::capTune | 
Internal capacitance tuning.
        Definition at line
        
         291
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::disOnDemand | 
Disable on-demand requests.
        Definition at line
        
         298
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::failDetEM4WUEn | 
EM4 wakeup on failure enable.
        Definition at line
        
         296
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::failDetEn | 
Oscillator failure detection enable.
        Definition at line
        
         297
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::forceEn | 
| uint8_t CMU_LFXOInit_TypeDef::gain | 
| bool CMU_LFXOInit_TypeDef::highAmplitudeEn | 
| CMU_LfxoOscMode_TypeDef CMU_LFXOInit_TypeDef::mode | 
| bool CMU_LFXOInit_TypeDef::regLock | 
| CMU_LfxoStartupDelay_TypeDef CMU_LFXOInit_TypeDef::timeout | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_cmu.h