IADC_CFG_TypeDef Struct ReferenceDevices > IADC
IADC CFG Register Group Declaration.
Definition at line
48
of file
efr32mg21_iadc.h
.
#include <
efr32mg21_iadc.h
>
Data Fields |
|
| __IOM uint32_t | CFG |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | SCALE |
| __IOM uint32_t | SCHED |
Field Documentation
| __IOM uint32_t IADC_CFG_TypeDef::CFG |
Configuration
Definition at line
49
of file
efr32mg21_iadc.h
.
Referenced by IADC_init() , and IADC_reset() .
| uint32_t IADC_CFG_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
efr32mg21_iadc.h
.
| __IOM uint32_t IADC_CFG_TypeDef::SCALE |
Scaling
Definition at line
51
of file
efr32mg21_iadc.h
.
Referenced by IADC_init() , and IADC_reset() .
| __IOM uint32_t IADC_CFG_TypeDef::SCHED |
Scheduling
Definition at line
52
of file
efr32mg21_iadc.h
.
Referenced by IADC_init() , and IADC_reset() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_iadc.h