IADC_InitScan_t Struct ReferenceEMLIB > IADC
IADC scan init structure
Definition at line
699
of file
em_iadc.h
.
#include <
em_iadc.h
>
Data Fields |
|
| IADC_Alignment_t | alignment |
| uint8_t | dataValidLevel |
| bool | fifoDmaWakeup |
| bool | showId |
| bool | start |
| IADC_TriggerAction_t | triggerAction |
| IADC_TriggerSel_t | triggerSelect |
Field Documentation
| IADC_Alignment_t IADC_InitScan_t::alignment |
Alignment of data in FIFO.
Definition at line
700
of file
em_iadc.h
.
Referenced by IADC_initScan() .
| uint8_t IADC_InitScan_t::dataValidLevel |
Data valid level before requesting DMA transfer.
Definition at line
702
of file
em_iadc.h
.
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::fifoDmaWakeup |
Wake-up DMA when FIFO reaches data valid level.
Definition at line
703
of file
em_iadc.h
.
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::showId |
Tag FIFO entry with scan table entry id.
Definition at line
701
of file
em_iadc.h
.
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::start |
| IADC_TriggerAction_t IADC_InitScan_t::triggerAction |
| IADC_TriggerSel_t IADC_InitScan_t::triggerSelect |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_iadc.h