Cluster Commands: Configuration Cluster

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_SET_TOKEN
zcl ota-config setToken [token:2] [data:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_LOCK
zcl ota-config lock
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_READ
zcl ota-config read [token:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_UNLOCK
zcl ota-config unlock [data:-1]

Detailed Description

This group describes the CLI commands for the Configuration Cluster cluster. Listed below is a description of the cluster:

This cluster allows for the OTA configuration of firmware parameters.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_LOCK

#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_LOCK

zcl ota-config lock

  • Command to lock the token values.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_READ

#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_READ

zcl ota-config read [token:2]

  • Command to read a token value.
    • token - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_SET_TOKEN

#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_SET_TOKEN

zcl ota-config setToken [token:2] [data:-1]

  • Command to write a token value over the air.
    • token - INT16U
    • data - OCTET_STRING

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_UNLOCK

#define EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_UNLOCK

zcl ota-config unlock [data:-1]

  • Command to unlock tokens with a device-specific password (if allowed).
    • data - OCTET_STRING