EmberNetworkInitStruct Struct Reference

Defines the network initialization configuration that should be used when ::emberNetworkInit() is called by the application.

#include < ember-types.h >

Data Fields

EmberNetworkInitBitmask bitmask

Defines the network initialization configuration that should be used when ::emberNetworkInit() is called by the application.

Field Documentation

◆ bitmask

EmberNetworkInitBitmask EmberNetworkInitStruct::bitmask

The documentation for this struct was generated from the following file:
  • ember-types.h