#include < af-types.h >

Data Fields

uint8_t siteId [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1]
uint32_t implementationDateTime
uint32_t issuerEventId

Field Documentation

◆ implementationDateTime

uint32_t EmberAfDeviceManagementSiteId::implementationDateTime

◆ issuerEventId

uint32_t EmberAfDeviceManagementSiteId::issuerEventId

◆ siteId

uint8_t EmberAfDeviceManagementSiteId::siteId[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1]

The documentation for this struct was generated from the following file:
  • af-types.h