Plugin Commands: ZigBee Light Link (ZLL) Commissioning

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ABORT
plugin zll-commissioning abort
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CANCEL_RX_ON
plugin zll-commissioning cancel-rx-on
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CHANNEL
plugin zll-commissioning channel [channel:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_DISABLE
plugin zll-commissioning disable
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENABLE
plugin zll-commissioning enable
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENDPOINTS
plugin zll-commissioning endpoints [destination:2] [sourceEndpoint:1] [destinationEndpoint:1] [startIndex:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_FORM
plugin zll-commissioning form [channel:1] [power:1] [panId:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_GROUPS
plugin zll-commissioning groups [destination:2] [sourceEndpoint:1] [destinationEndpoint:1] [startIndex:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_IDENTIFY
plugin zll-commissioning identify [identifyDurationDs:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_INFO
plugin zll-commissioning info [destination:2] [sourceEndpoint:1] [destinationEndpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_JOINABLE
plugin zll-commissioning joinable
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_LINK
plugin zll-commissioning link
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_MASK
plugin zll-commissioning mask [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NORESET_NFN
plugin zll-commissioning noreset-nfn
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NOTOUCHLINK_NFN
plugin zll-commissioning notouchlink-nfn
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RESET
plugin zll-commissioning reset
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RX_ON_ACTIVE
plugin zll-commissioning rx-on-active
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_DEVICE
plugin zll-commissioning scan device
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_IDENTIFY
plugin zll-commissioning scan identify
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_RESET
plugin zll-commissioning scan reset
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SECONDARY_CHANNEL
plugin zll-commissioning secondary-channel [channel:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SET_RX_ON
plugin zll-commissioning set-rx-on [duration:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_STATUS
plugin zll-commissioning status
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_TOKENS
plugin zll-commissioning tokens
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_UNUSED
plugin zll-commissioning unused

Detailed Description

The ZigBee Light Link (ZLL) Commissioning Plugin contributes several commands to the application framework's CLI. These commands are used for forming and managing a ZLL network.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ABORT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ABORT

plugin zll-commissioning abort

  • Abort the touch link procedure.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CANCEL_RX_ON

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CANCEL_RX_ON

plugin zll-commissioning cancel-rx-on

  • Cancel Rx On When Idle.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CHANNEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_CHANNEL

plugin zll-commissioning channel [channel:1]

  • Set the scan channel used by the ZLL Commissioning plugin.
    • channel - INT8U - The primary channel to be used.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_DISABLE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_DISABLE

plugin zll-commissioning disable

  • Disable touchlinking. This will override the notouchlink-nfn and noreset-nfn commands.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENABLE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENABLE

plugin zll-commissioning enable

  • Enable touchlinking. This will override the notouchlink-nfn and noreset-nfn commands.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENDPOINTS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_ENDPOINTS

plugin zll-commissioning endpoints [destination:2] [sourceEndpoint:1] [destinationEndpoint:1] [startIndex:1]

  • Send a GetEndpointListRequest to a server.
    • destination - INT16U - The network address of the device to which the request will be sent.
    • sourceEndpoint - INT8U - The source endpoint from which the request will be sent.
    • destinationEndpoint - INT8U - The destination endpoint to which the request will be sent.
    • startIndex - INT8U - The endpoint index at which to start retreiving data.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_FORM

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_FORM

plugin zll-commissioning form [channel:1] [power:1] [panId:2]

  • Form a ZLL network.
    • channel - INT8U - The channel on which to form the network.
    • power - INT8S - The power setting for network transmissions.
    • panId - INT16U - The PAN identifier for the network.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_GROUPS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_GROUPS

plugin zll-commissioning groups [destination:2] [sourceEndpoint:1] [destinationEndpoint:1] [startIndex:1]

  • Send a GroupIdentifiersRequest to a server.
    • destination - INT16U - The network address of the device to which the request will be sent.
    • sourceEndpoint - INT8U - The source endpoint from which the request will be sent.
    • destinationEndpoint - INT8U - The destination endpoint to which the request will be sent.
    • startIndex - INT8U - The group table index at which to start retreiving data.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_IDENTIFY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_IDENTIFY

plugin zll-commissioning identify [identifyDurationDs:2]

  • Set the duration that a target device should remain in identify mode during touch linking.
    • identifyDurationDs - INT16U - The duration (in tenths of a second) of identify mode or 0xFFFF to indicate that the target should use its own application-specific duration.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_INFO

plugin zll-commissioning info [destination:2] [sourceEndpoint:1] [destinationEndpoint:1]

  • Send an EndpointInformationRequest to a client.
    • destination - INT16U - The network address of the device to which the request will be sent.
    • sourceEndpoint - INT8U - The source endpoint from which the request will be sent.
    • destinationEndpoint - INT8U - The destination endpoint to which the request will be sent.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_JOINABLE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_JOINABLE

plugin zll-commissioning joinable

  • Scan for joinable networks and attempt to join if a network is found.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_LINK

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_LINK

plugin zll-commissioning link

  • Initiate the touch link procedure.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_MASK

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_MASK

plugin zll-commissioning mask [index:1]

  • Set the scan channel set used by the ZLL Commissioning plugin. An index of 0 sets the primary ZLL channel set, 1 is the +1 channel set, 2 is the +2 channel set, 3 is the +3 channel set, and 4 is all ZigBee channels.
    • index - INT8U - The index of the channel mask to be used.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NORESET_NFN

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NORESET_NFN

plugin zll-commissioning noreset-nfn

  • Disable reset for an NFN device on a centralized security network.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NOTOUCHLINK_NFN

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_NOTOUCHLINK_NFN

plugin zll-commissioning notouchlink-nfn

  • Disable touchlinking (stealing) for an NFN device.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RESET

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RESET

plugin zll-commissioning reset

  • Reset the local device to factory new.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RX_ON_ACTIVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_RX_ON_ACTIVE

plugin zll-commissioning rx-on-active

  • Get Rx On When Idle status.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_DEVICE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_DEVICE

plugin zll-commissioning scan device

  • Initiate a touch link for the purpose of retrieving information about a target device.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_IDENTIFY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_IDENTIFY

plugin zll-commissioning scan identify

  • Initiate a touch link for the purpose of causing a target device to identify itself.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_RESET

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SCAN_RESET

plugin zll-commissioning scan reset

  • Initiate a touch link for the purpose of resetting a target device.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SECONDARY_CHANNEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SECONDARY_CHANNEL

plugin zll-commissioning secondary-channel [channel:1]

  • Set the scan channel used by the ZLL Commissioning plugin.
    • channel - INT8U - The secondary channel to be used.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SET_RX_ON

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_SET_RX_ON

plugin zll-commissioning set-rx-on [duration:4]

  • Set Rx On When Idle duration.
    • duration - INT32U - The duration for the Rx On period.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_STATUS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_STATUS

plugin zll-commissioning status

  • Print the ZLL channel set and tokens.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_TOKENS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_TOKENS

plugin zll-commissioning tokens

  • Print the ZLL tokens.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_UNUSED

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ZLL_COMMISSIONING_PLUGIN_ZLL_COMMISSIONING_UNUSED

plugin zll-commissioning unused

  • Scan for an unused PAN identifier and form a new ZLL network.