EmberAfPluginMessagingClientMessage Struct Reference

#include < af-types.h >

Data Fields

bool valid
bool active
EmberAfPluginEsiManagementBitmask esiBitmask
uint8_t clientEndpoint
uint32_t messageId
uint8_t messageControl
uint32_t startTime
uint32_t endTime
uint16_t durationInMinutes
uint8_t message [ EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE +1]

Field Documentation

◆ active

bool EmberAfPluginMessagingClientMessage::active

◆ clientEndpoint

uint8_t EmberAfPluginMessagingClientMessage::clientEndpoint

◆ durationInMinutes

uint16_t EmberAfPluginMessagingClientMessage::durationInMinutes

◆ endTime

uint32_t EmberAfPluginMessagingClientMessage::endTime

◆ esiBitmask

EmberAfPluginEsiManagementBitmask EmberAfPluginMessagingClientMessage::esiBitmask

◆ message

uint8_t EmberAfPluginMessagingClientMessage::message[ EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE +1]

◆ messageControl

uint8_t EmberAfPluginMessagingClientMessage::messageControl

◆ messageId

uint32_t EmberAfPluginMessagingClientMessage::messageId

◆ startTime

uint32_t EmberAfPluginMessagingClientMessage::startTime

◆ valid

bool EmberAfPluginMessagingClientMessage::valid

The documentation for this struct was generated from the following file:
  • af-types.h