Plugin Commands: Wwah Connectivity Manager

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_DISABLE
plugin wwah-connectivity-manager disable [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_ENABLE
plugin wwah-connectivity-manager enable [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_INFO
plugin wwah-connectivity-manager info
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_MIN_RSSI
plugin wwah-connectivity-manager min-rssi [rssi:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PARENT_RECOVERY
plugin wwah-connectivity-manager parent-recovery [enabled:1] [badParentRejoinPeriod:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_SHOW
plugin wwah-connectivity-manager show

Detailed Description

The wwah-connectivity-manager plugin CLI contains commands to interact with the connectivity manager.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_DISABLE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_DISABLE

plugin wwah-connectivity-manager disable [endpoint:1]

  • Disable the WWAH Connectivity Manager rejoin algorithm.
    • endpoint - INT8U - The endpoint which contains WWAH cluster

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_ENABLE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_ENABLE

plugin wwah-connectivity-manager enable [endpoint:1]

  • Enable the WWAH Connectivity Manager rejoin algorithm.
    • endpoint - INT8U - The endpoint which contains WWAH cluster

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_INFO

plugin wwah-connectivity-manager info

  • Print information about the WWAH Connectivity Manager state.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_MIN_RSSI

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_MIN_RSSI

plugin wwah-connectivity-manager min-rssi [rssi:1]

  • Sets minimum acceptable RSSI for receiving packets on a SoC WWAH-enabled device
    • rssi - INT8S - min acceptable Rssi value for receiving packets

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PARENT_RECOVERY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PARENT_RECOVERY

plugin wwah-connectivity-manager parent-recovery [enabled:1] [badParentRejoinPeriod:2]

  • Disable/enable the WWAH bad parent recovery. And set the bad parent check and rejoin period (min), if enabled.
    • enabled - INT8U - Disable ==0, enable == 1, the WWAH bad parent recovery
    • badParentRejoinPeriod - INT16U - the Period of time after which, we check if a parent is bad and try rejoin if so. 0 means use the default value of 24 * 60 mins.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_SHOW

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_CONNECTIVITY_MANAGER_PLUGIN_WWAH_CONNECTIVITY_MANAGER_SHOW

plugin wwah-connectivity-manager show

  • Shows the WWAH Connectivity Manager rejoin algorithm's parameters.