Plugin Commands: CLI password protection

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CLI_PASSWORD_PROTECTION_PLUGIN_CLI_PASSWORD_PROTECTION_CHANGE_PASSWORD
plugin cli-password-protection changePassword [newPass:4]

Detailed Description

The CLI-password-protection plugin contributes one command to the application framework's CLI.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CLI_PASSWORD_PROTECTION_PLUGIN_CLI_PASSWORD_PROTECTION_CHANGE_PASSWORD

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CLI_PASSWORD_PROTECTION_PLUGIN_CLI_PASSWORD_PROTECTION_CHANGE_PASSWORD

plugin cli-password-protection changePassword [newPass:4]

  • This command is used to change the current password.
    • newPass - INT32U - The new password needs to be a number between 1 and 0xFFFFFFFE