Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_STOP
zcl poll-control stop
#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_LONG
zcl poll-control long [newLongPollInterval:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_SHORT
zcl poll-control short [newShortPollInterval:2]

Detailed Description

This group describes the CLI commands for the Poll Control cluster. Listed below is a description of the cluster:

This cluster provides a mechanism for the management of an end device's MAC Data Poll rate. For the purposes of this cluster, the term "poll" always refers to the sending of a MAC Data Poll from the end device to the end device's parent.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_LONG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_LONG

zcl poll-control long [newLongPollInterval:4]

  • The Set Long Poll Interval command is used to set the read only Long Poll Interval Attribute.
    • newLongPollInterval - INT32U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_SHORT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_SHORT

zcl poll-control short [newShortPollInterval:2]

  • The Set Short Poll Interval command is used to set the read only Short Poll Interval Attribute.
    • newShortPollInterval - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_STOP

zcl poll-control stop

  • The Fast Poll Stop command is used to stop the fast poll mode initiated by the Check-in response.