Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ACTIVE_PHY
plugin antenna get-active-phy
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_RX_MODE
plugin antenna get-antenna-rx-mode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_TX_MODE
plugin antenna get-antenna-tx-mode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_RX_MODE
plugin antenna set-antenna-rx-mode [mode:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_TX_MODE
plugin antenna set-antenna-tx-mode [mode:1]

Detailed Description

The antenna commands allow you run-time reconfiguration of the antenna plugin

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ACTIVE_PHY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ACTIVE_PHY

plugin antenna get-active-phy

  • Get the active RAIL PHY

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_RX_MODE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_RX_MODE

plugin antenna get-antenna-rx-mode

  • Get the RX antenna mode

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_TX_MODE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_TX_MODE

plugin antenna get-antenna-tx-mode

  • Get the TX antenna mode

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_RX_MODE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_RX_MODE

plugin antenna set-antenna-rx-mode [mode:1]

  • Set the RX antenna mode
    • mode - INT8U - Configure the RX antenna mode(0-don't switch,1-primary,2-secondary,3-RX antenna diversity).

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_TX_MODE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_TX_MODE

plugin antenna set-antenna-tx-mode [mode:1]

  • Set the TX antenna mode
    • mode - INT8U - Configure the TX antenna mode(0-don't switch,1-primary,2-secondary,3-TX antenna diversity).