#include < af-types.h >

Data Fields

uint8_t cin [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH +1]
uint32_t implementationDateTime
uint32_t issuerEventId

Field Documentation

◆ cin

uint8_t EmberAfDeviceManagementCIN::cin[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH +1]

◆ implementationDateTime

uint32_t EmberAfDeviceManagementCIN::implementationDateTime

◆ issuerEventId

uint32_t EmberAfDeviceManagementCIN::issuerEventId

The documentation for this struct was generated from the following file:
  • af-types.h