Plugin Commands: Barrier Control Server Cluster

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_CLOSE
plugin barrier-control-server close [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_FAILED_COMMUNICATION
plugin barrier-control-server failed-communication [endpoint:1] [setOrClear:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_OPEN
plugin barrier-control-server open [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_POSITION_FAILURE
plugin barrier-control-server position-failure [endpoint:1] [setOrClear:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_REMOTE_LOCKOUT
plugin barrier-control-server remote-lockout [endpoint:1] [setOrClear:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_STATUS
plugin barrier-control-server status [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_TAMPER_DETECTED
plugin barrier-control-server tamper-detected [endpoint:1] [setOrClear:1]

Detailed Description

Commands pertaining to the Silicon Labs Barrier Control server cluster.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_CLOSE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_CLOSE

plugin barrier-control-server close [endpoint:1]

  • Notify the plugin that the barrier has been closed manually.
    • endpoint - INT8U - The endpoint on which the barrier has been closed

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_FAILED_COMMUNICATION

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_FAILED_COMMUNICATION

plugin barrier-control-server failed-communication [endpoint:1] [setOrClear:1]

  • Simulate or clear a failed communication event on the barrier (i.e., set or clear the FailedCommunication bit in the SafetyStatus attribute).
    • endpoint - INT8U - The endpoint on which to simulate this failed communication event
    • setOrClear - INT8U - Whether to set (1) or clear (0) the failed communication state

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_OPEN

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_OPEN

plugin barrier-control-server open [endpoint:1]

  • Notify the plugin that the barrier has been opened manually.
    • endpoint - INT8U - The endpoint on which the barrier has been opened

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_POSITION_FAILURE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_POSITION_FAILURE

plugin barrier-control-server position-failure [endpoint:1] [setOrClear:1]

  • Simulate or clear a position failure event on the barrier (i.e., set or clear the PositionFailure bit in the SafetyStatus attribute).
    • endpoint - INT8U - The endpoint on which to simulate this position failure event
    • setOrClear - INT8U - Whether to set (1) or clear (0) the position failure state

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_REMOTE_LOCKOUT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_REMOTE_LOCKOUT

plugin barrier-control-server remote-lockout [endpoint:1] [setOrClear:1]

  • Simulate or clear a remote lockout event on the barrier (i.e., set or clear the RemoteLockout bit in the SafetyStatus attribute).
    • endpoint - INT8U - The endpoint on which to simulate this remote lockout event
    • setOrClear - INT8U - Whether to set (1) or clear (0) the remove lockout state

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_STATUS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_STATUS

plugin barrier-control-server status [endpoint:1]

  • Prints out the status of the Barrier Control server cluster implementation.
    • endpoint - INT8U - The endpoint from which to receive status

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_TAMPER_DETECTED

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_TAMPER_DETECTED

plugin barrier-control-server tamper-detected [endpoint:1] [setOrClear:1]

  • Simulate or clear a tamper detected event on the barrier (i.e., set or clear the TamperDetected bit in the SafetyStatus attribute).
    • endpoint - INT8U - The endpoint on which to simulate this tamper detected event
    • setOrClear - INT8U - Whether to set (1) or clear (0) the tamper detected state