A struct containing endpoint information about a device.

#include < af-types.h >

Data Fields

EmberEUI64 eui64
EmberAfEndpointInfoStruct endpoints [ EMBER_AF_MAX_ENDPOINTS_PER_DEVICE ]
EmberAfDeviceDiscoveryStatus status
uint8_t discoveryFailures
uint8_t capabilities
uint8_t endpointCount
uint8_t stackRevision

A struct containing endpoint information about a device.

Field Documentation

◆ capabilities

uint8_t EmberAfDeviceInfo::capabilities

◆ discoveryFailures

uint8_t EmberAfDeviceInfo::discoveryFailures

◆ endpointCount

uint8_t EmberAfDeviceInfo::endpointCount

◆ endpoints

◆ eui64

EmberEUI64 EmberAfDeviceInfo::eui64

◆ stackRevision

uint8_t EmberAfDeviceInfo::stackRevision

◆ status

EmberAfDeviceDiscoveryStatus EmberAfDeviceInfo::status

The documentation for this struct was generated from the following file:
  • af-types.h