EmberAfDeviceManagementTenancy Struct Reference

#include < af-types.h >

Data Fields

uint32_t providerId
uint32_t issuerEventId
uint8_t tariffType
uint32_t implementationDateTime
uint32_t tenancy

Field Documentation

◆ implementationDateTime

uint32_t EmberAfDeviceManagementTenancy::implementationDateTime

◆ issuerEventId

uint32_t EmberAfDeviceManagementTenancy::issuerEventId

◆ providerId

uint32_t EmberAfDeviceManagementTenancy::providerId

◆ tariffType

uint8_t EmberAfDeviceManagementTenancy::tariffType

◆ tenancy

uint32_t EmberAfDeviceManagementTenancy::tenancy

The documentation for this struct was generated from the following file:
  • af-types.h