This structure is used define an interpan message that will be accepted by the interpan filters.

#include < af-types.h >

Data Fields

EmberAfProfileId profileId
EmberAfClusterId clusterId
uint8_t commandId
EmberAfAllowedInterpanOptions options

This structure is used define an interpan message that will be accepted by the interpan filters.

Field Documentation

◆ clusterId

EmberAfClusterId EmberAfAllowedInterPanMessage::clusterId

◆ commandId

uint8_t EmberAfAllowedInterPanMessage::commandId

◆ options

EmberAfAllowedInterpanOptions EmberAfAllowedInterPanMessage::options

◆ profileId

EmberAfProfileId EmberAfAllowedInterPanMessage::profileId

The documentation for this struct was generated from the following file:
  • af-types.h