A structure used to store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is
EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID
, the entry is unused.
#include <
af-types.h
>
A structure used to store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is
EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID
, the entry is unused.
◆
endpoint
|
uint8_t EmberAfSceneTableEntry::endpoint
|
◆
groupId
|
uint16_t EmberAfSceneTableEntry::groupId
|
◆
sceneId
|
uint8_t EmberAfSceneTableEntry::sceneId
|
◆
transitionTime
|
uint16_t EmberAfSceneTableEntry::transitionTime
|
◆
transitionTime100ms
|
uint8_t EmberAfSceneTableEntry::transitionTime100ms
|
The documentation for this struct was generated from the following file: