Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_CLEAR_COUNTERS
plugin throughput clear-counters
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_COUNTERS
plugin throughput print-counters
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_PARAMETERS
plugin throughput print-parameters
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_RESULT
plugin throughput print-result
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_ALL
plugin throughput set-all [nodeId:2] [count:2] [interval:2] [packet:1] [inflight_count:1] [apsOptions:2] [timeout:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_OFF
plugin throughput set-aps-ack-off
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_ON
plugin throughput set-aps-ack-on
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_COUNT
plugin throughput set-count [count:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_DESTINATION
plugin throughput set-destination [nodeId:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INFLIGHT
plugin throughput set-inflight [inflight_count:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INTERVAL
plugin throughput set-interval [interval:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_PACKET_SIZE
plugin throughput set-packet-size [packet:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_TIMEOUT
plugin throughput set-timeout [timeout:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_START
plugin throughput start
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_STOP
plugin throughput stop

Detailed Description

The throughput commands allow you to test your application's network throughput

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_CLEAR_COUNTERS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_CLEAR_COUNTERS

plugin throughput clear-counters

  • Clear all the stack counters

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_COUNTERS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_COUNTERS

plugin throughput print-counters

  • Print the stack counters

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_PARAMETERS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_PARAMETERS

plugin throughput print-parameters

  • Print all the test parameters

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_RESULT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_RESULT

plugin throughput print-result

  • Show the results of the last test.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_ALL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_ALL

plugin throughput set-all [nodeId:2] [count:2] [interval:2] [packet:1] [inflight_count:1] [apsOptions:2] [timeout:4]

  • Set all parameters: Destination Count Interval packetLength maxInFlight testTimeout
    • nodeId - INT16U - Destination nodeId
    • count - INT16U - Packets to send
    • interval - INT16U - Interval in ms
    • packet - INT8U - Packet length in bytes
    • inflight_count - INT8U - Packets in flight
    • apsOptions - INT16U - APS Options
    • timeout - INT32U - Timeout in ms

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_OFF

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_OFF

plugin throughput set-aps-ack-off

  • Turn off APS acks

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_ON

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_ON

plugin throughput set-aps-ack-on

  • Turn on APS acks

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_COUNT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_COUNT

plugin throughput set-count [count:2]

  • Set the number of packets to send
    • count - INT16U - Packets to send

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_DESTINATION

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_DESTINATION

plugin throughput set-destination [nodeId:2]

  • Set the destination nodeId
    • nodeId - INT16U - Destination nodeId

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INFLIGHT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INFLIGHT

plugin throughput set-inflight [inflight_count:1]

  • Set the number of packets in flight during the test.
    • inflight_count - INT8U - Packets in flight

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INTERVAL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INTERVAL

plugin throughput set-interval [interval:2]

  • Set the interval
    • interval - INT16U - Interval in ms

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_PACKET_SIZE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_PACKET_SIZE

plugin throughput set-packet-size [packet:1]

  • Set the packet length
    • packet - INT8U - Packet length in bytes

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_TIMEOUT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_TIMEOUT

plugin throughput set-timeout [timeout:4]

  • Set the test timeout
    • timeout - INT32U - Timeout in ms

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_START

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_START

plugin throughput start

  • Start the throughput test.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_STOP

plugin throughput stop

  • Abort the test while running.