EmberVersion Struct Reference

A version structure containing all version information.

#include < ember-types.h >

Data Fields

uint16_t build
uint8_t major
uint8_t minor
uint8_t patch
uint8_t special
EmberVersionType type

A version structure containing all version information.

Field Documentation

◆ build

uint16_t EmberVersion::build

◆ major

uint8_t EmberVersion::major

◆ minor

uint8_t EmberVersion::minor

◆ patch

uint8_t EmberVersion::patch

◆ special

uint8_t EmberVersion::special

◆ type

EmberVersionType EmberVersion::type

The documentation for this struct was generated from the following file:
  • ember-types.h