#include < af-types.h >

Data Fields

uint8_t * gbzCommands
uint16_t gbzCommandsLength
uint8_t * gbzCommandsResponse
uint16_t gbzCommandsResponseLength
uint16_t messageCode

Field Documentation

◆ gbzCommands

uint8_t* EmberAfGpfMessage::gbzCommands

◆ gbzCommandsLength

uint16_t EmberAfGpfMessage::gbzCommandsLength

◆ gbzCommandsResponse

uint8_t* EmberAfGpfMessage::gbzCommandsResponse

◆ gbzCommandsResponseLength

uint16_t EmberAfGpfMessage::gbzCommandsResponseLength

◆ messageCode

uint16_t EmberAfGpfMessage::messageCode

The documentation for this struct was generated from the following file:
  • af-types.h