EmberSmacData Struct Reference

This data structure contains the Shared Message Authentication Code (SMAC) data that is used for Certificate Based Key Exchange (CBKE).

#include < ember-types.h >

Data Fields

uint8_t contents [ EMBER_SMAC_SIZE ]

This data structure contains the Shared Message Authentication Code (SMAC) data that is used for Certificate Based Key Exchange (CBKE).

Field Documentation

◆ contents

uint8_t EmberSmacData::contents[ EMBER_SMAC_SIZE ]

The documentation for this struct was generated from the following file:
  • ember-types.h