Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_FORM
plugin network-creator form [useCentralizedSecurity:1] [panId:2] [radioTxPower:1] [channel:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_ADD
plugin network-creator mask add [mask:1] [channel:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SET
plugin network-creator mask set [mask:1] [newChannelMask:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SUBTRACT
plugin network-creator mask subtract [mask:1] [channel:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_START
plugin network-creator start [useCentralizedSecurity:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STATUS
plugin network-creator status
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STOP
plugin network-creator stop

Detailed Description

Commands pertaining to network creation with the Network Creator plugin.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_FORM

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_FORM

plugin network-creator form [useCentralizedSecurity:1] [panId:2] [radioTxPower:1] [channel:1]

  • Form a network with specified parameters.
    • useCentralizedSecurity - BOOLEAN - Whether or not to form a centralized network. If this value is false, the device will attempt to join a distributed network.
    • panId - INT16U - PanID of the network to be formed
    • radioTxPower - INT8S - Tx power of the network to be formed
    • channel - INT8U - channel of the network to be formed

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_ADD

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_ADD

plugin network-creator mask add [mask:1] [channel:4]

  • Add a channel to the channel mask of choice.
    • mask - INT8U - The mask of choice to which to add the channel. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
    • channel - INT32U - The channel to add to the channel mask.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SET

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SET

plugin network-creator mask set [mask:1] [newChannelMask:4]

  • Set a channel mask.
    • mask - INT8U - The mask of choice to set. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
    • newChannelMask - INT32U - The bit mask to which to set the chosen channel mask.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SUBTRACT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SUBTRACT

plugin network-creator mask subtract [mask:1] [channel:4]

  • Subtract a channel from the channel mask of choice.
    • mask - INT8U - The mask of choice from which to subtract the channel. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
    • channel - INT32U - The channel to subtract from the channel mask.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_START

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_START

plugin network-creator start [useCentralizedSecurity:1]

  • Starts the network formation process.
    • useCentralizedSecurity - BOOLEAN - Whether or not to form a centralized network. If this value is false, the device will attempt to join a distributed network.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STATUS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STATUS

plugin network-creator status

  • Print the status of the network-creator plugin.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STOP

plugin network-creator stop

  • Stops the network formation process.