This structure is an in-memory representation of the Over-the-air header data that resides on disk. It is not a byte-for-byte copy.

#include < af-types.h >

Data Fields

uint16_t headerVersion
uint16_t headerLength
uint16_t fieldControl
uint16_t manufacturerId
uint16_t imageTypeId
uint32_t firmwareVersion
uint16_t zigbeeStackVersion
uint8_t headerString [ EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH +1]
The spec. does NOT require that the string be NULL terminated in the header stored on disk. Therefore we make sure we can support a 32-character string without a NULL terminator by adding +1 in the data structure.
uint32_t imageSize
When reading the header this will be the complete length of the file. When writing the header, this must be set to the length of the MFG image data portion including all tags.
uint8_t securityCredentials
The remaining four fields are optional. The field control should be checked to determine if their values are valid.
union {
uint8_t EUI64 [ EUI64_SIZE ]
uint8_t UID [ UID_SIZE ]
} upgradeFileDestination
uint16_t minimumHardwareVersion
uint16_t maximumHardwareVersion

This structure is an in-memory representation of the Over-the-air header data that resides on disk. It is not a byte-for-byte copy.

Field Documentation

◆ EUI64

uint8_t EmberAfOtaHeader::EUI64[ EUI64_SIZE ]

◆ fieldControl

uint16_t EmberAfOtaHeader::fieldControl

◆ firmwareVersion

uint32_t EmberAfOtaHeader::firmwareVersion

◆ headerLength

uint16_t EmberAfOtaHeader::headerLength

◆ headerString

uint8_t EmberAfOtaHeader::headerString[ EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH +1]

The spec. does NOT require that the string be NULL terminated in the header stored on disk. Therefore we make sure we can support a 32-character string without a NULL terminator by adding +1 in the data structure.

◆ headerVersion

uint16_t EmberAfOtaHeader::headerVersion

◆ imageSize

uint32_t EmberAfOtaHeader::imageSize

When reading the header this will be the complete length of the file. When writing the header, this must be set to the length of the MFG image data portion including all tags.

◆ imageTypeId

uint16_t EmberAfOtaHeader::imageTypeId

◆ manufacturerId

uint16_t EmberAfOtaHeader::manufacturerId

◆ maximumHardwareVersion

uint16_t EmberAfOtaHeader::maximumHardwareVersion

◆ minimumHardwareVersion

uint16_t EmberAfOtaHeader::minimumHardwareVersion

◆ securityCredentials

uint8_t EmberAfOtaHeader::securityCredentials

The remaining four fields are optional. The field control should be checked to determine if their values are valid.

◆ UID

uint8_t EmberAfOtaHeader::UID[ UID_SIZE ]

◆ upgradeFileDestination

union { ... } EmberAfOtaHeader::upgradeFileDestination

◆ zigbeeStackVersion

uint16_t EmberAfOtaHeader::zigbeeStackVersion

The documentation for this struct was generated from the following file:
  • af-types.h