Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT
plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER
plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]

Detailed Description

The EZ-Mode Commissioning plugin contributes several commands to the application framework's CLI.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT

plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]

  • Start EZ-Mode client commissioning.
    • endpoint - INT8U - The local endpoint.
    • direction - INT8U - ::EMBER_AF_EZMODE_COMMISSIONING_SERVER_TO_CLIENT or ::EMBER_AF_EZMODE_COMMISSIONING_CLIENT_TO_SERVER.
    • clusterIds - INT16U - A list of cluster ids.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER

plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]

  • Start EZ-Mode server commissioning.
    • endpoint - INT8U - The local endpoint.
    • identifyTimeS - INT16U - The identify time in seconds.