EmberChildData Struct Reference
This structure contains information about child nodes.
#include <
ember-types.h
>
Data Fields |
|
| EmberEUI64 | eui64 |
| EmberNodeType | type |
| EmberNodeId | id |
| uint8_t | phy |
| uint8_t | power |
| uint8_t | timeout |
This structure contains information about child nodes.
Field Documentation
◆ eui64
| EmberEUI64 EmberChildData::eui64 |
◆ id
| EmberNodeId EmberChildData::id |
◆ phy
| uint8_t EmberChildData::phy |
◆ power
| uint8_t EmberChildData::power |
◆ timeout
| uint8_t EmberChildData::timeout |
◆ type
| EmberNodeType EmberChildData::type |
The documentation for this struct was generated from the following file:
-
ember-types.h