EmberEventData Struct Reference

Complete events with a control and a handler procedure.

#include < ember-types.h >

Data Fields

EmberEventControl * control
void(* handler )(void)

Complete events with a control and a handler procedure.

An application typically creates an array of events along with their handlers. The main loop passes the array to ::emberRunEvents() to call the handlers of any events whose time has arrived.

Field Documentation

◆ control

EmberEventControl * EmberEventData::control

The control structure for the event.

◆ handler

void(* EmberEventData::handler) (void)

The procedure to call when the event fires.


The documentation for this struct was generated from the following file:
  • ember-types.h