Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_LOG_CATCHUPS_IN_PROGRESS
plugin gas-proxy-function print-log-catchups-in-progress
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_SUPPORTED_USE_CASES
plugin gas-proxy-function print-supported-use-cases
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_FUTURE_DATED_MSG
plugin gas-proxy-function simulate-future-dated-msg
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG
plugin gas-proxy-function simulate-gbz-msg [useCase:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG_CREATION
plugin gas-proxy-function simulate-gbz-msg-creation

Detailed Description

The reporting plugin contributes several CLI commands to the application framework to be used in creating and managing Gas Proxy Function functionality on the device.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_LOG_CATCHUPS_IN_PROGRESS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_LOG_CATCHUPS_IN_PROGRESS

plugin gas-proxy-function print-log-catchups-in-progress

  • Print the number of logs that are currently catching up with missed entries.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_SUPPORTED_USE_CASES

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_SUPPORTED_USE_CASES

plugin gas-proxy-function print-supported-use-cases

  • Print the list of supported use cases. The message code printed should be used with the simulate-gbz-msg command.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_FUTURE_DATED_MSG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_FUTURE_DATED_MSG

plugin gas-proxy-function simulate-future-dated-msg

  • Simulate transmission of a GBZ message to the Gas Proxy Function.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG

plugin gas-proxy-function simulate-gbz-msg [useCase:2]

  • Simulate transmission of a GBZ message to the Gas Proxy Function.
    • useCase - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG_CREATION

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG_CREATION

plugin gas-proxy-function simulate-gbz-msg-creation

  • Testing of GBZ message controller API.