EmberAfDeviceManagementUncontrolledFlowThreshold Struct Reference

#include < af-types.h >

Data Fields

uint16_t uncontrolledFlowThreshold
uint16_t multiplier
uint16_t divisor
uint16_t measurementPeriod
uint8_t unitOfMeasure
uint8_t stabilisationPeriod

Field Documentation

◆ divisor

uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::divisor

◆ measurementPeriod

uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::measurementPeriod

◆ multiplier

uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::multiplier

◆ stabilisationPeriod

uint8_t EmberAfDeviceManagementUncontrolledFlowThreshold::stabilisationPeriod

◆ uncontrolledFlowThreshold

uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::uncontrolledFlowThreshold

◆ unitOfMeasure

uint8_t EmberAfDeviceManagementUncontrolledFlowThreshold::unitOfMeasure

The documentation for this struct was generated from the following file:
  • af-types.h