Type describing the attribute default, min and max values.

#include < af-types.h >

Data Fields

EmberAfDefaultAttributeValue defaultValue
EmberAfDefaultAttributeValue minValue
EmberAfDefaultAttributeValue maxValue

Type describing the attribute default, min and max values.

This struct is required if the attribute mask specifies that this attribute has a known min and max values.

Field Documentation

◆ defaultValue

EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::defaultValue

Default value of the attribute.

◆ maxValue

EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::maxValue

Maximum allowed value.

◆ minValue

EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::minValue

Minimum allowed value


The documentation for this struct was generated from the following file:
  • af-types.h