Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CLOSE_TUNNEL
plugin comms-hub-function close-tunnel [dstEUI64:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CREATE_TUNNEL
plugin comms-hub-function create-tunnel [dstEUI64:8] [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_GET_TUNNEL_ENDPOINT
plugin comms-hub-function get-tunnel-endpoint [nodeId:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT
plugin comms-hub-function print
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT_SUPPORTED_USE_CASES
plugin comms-hub-function print-supported-use-cases
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SEND
plugin comms-hub-function send [dstEUI64:8] [payload:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SIMULATE_GBZ_MSG
plugin comms-hub-function simulate-gbz-msg [dstEUI64:8] [useCase:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_TIMEOUT
plugin comms-hub-function timeout [timeout:4]

Detailed Description

The comms-hub-function plugin contributes several CLI commands to the application framework to be used in configuring and managing the CHF.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CLOSE_TUNNEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CLOSE_TUNNEL

plugin comms-hub-function close-tunnel [dstEUI64:8]

  • Remove the tunnel for a given device.
    • dstEUI64 - IEEE_ADDRESS

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CREATE_TUNNEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CREATE_TUNNEL

plugin comms-hub-function create-tunnel [dstEUI64:8] [endpoint:1]

  • Create tunnel for the given device and endpoint.
    • dstEUI64 - IEEE_ADDRESS
    • endpoint - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_GET_TUNNEL_ENDPOINT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_GET_TUNNEL_ENDPOINT

plugin comms-hub-function get-tunnel-endpoint [nodeId:2]

  • Retrieve the tunneling endpoint for a given nodeId.
    • nodeId - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT

plugin comms-hub-function print

  • Prints the comms hub tunnel table.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT_SUPPORTED_USE_CASES

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT_SUPPORTED_USE_CASES

plugin comms-hub-function print-supported-use-cases

  • Print the list of supported use cases. The message code printed should be used with the simulate-gbz-msg command.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SEND

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SEND

plugin comms-hub-function send [dstEUI64:8] [payload:-1]

  • Send a message.
    • dstEUI64 - IEEE_ADDRESS
    • payload - OCTET_STRING

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SIMULATE_GBZ_MSG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SIMULATE_GBZ_MSG

plugin comms-hub-function simulate-gbz-msg [dstEUI64:8] [useCase:2]

  • Simulate transmission of a GBZ message to the Comms Hub Function.
    • dstEUI64 - IEEE_ADDRESS
    • useCase - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_TIMEOUT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_TIMEOUT

plugin comms-hub-function timeout [timeout:4]

  • Set the default sleepy message timeout.
    • timeout - INT32U