Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD
plugin address-table add [entry:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP
plugin address-table lookup [entry:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT
plugin address-table print
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE
plugin address-table remove [entry:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET
plugin address-table set [index:1] [eui64:8] [nodeId:2]

Detailed Description

This plugin provides a set of APIs and CLI commands for managing the address table

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD

plugin address-table add [entry:8]

  • Add an entry to the address table.
    • entry - IEEE_ADDRESS - Entry to be added.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP

plugin address-table lookup [entry:8]

  • Lookup an entry in the address table.
    • entry - IEEE_ADDRESS - Entry to be looked up.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT

plugin address-table print

  • Prints the address table.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE

plugin address-table remove [entry:8]

  • Remove an entry from the address table.
    • entry - IEEE_ADDRESS - Entry to be removed.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET

plugin address-table set [index:1] [eui64:8] [nodeId:2]

  • Set an entry in the address table according to the arguments specified
    • index - INT8U
    • eui64 - IEEE_ADDRESS
    • nodeId - INT16U