Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF
zcl identify off [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON
zcl identify on [endpoint:1] [time:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID
zcl identify id [identifyTime:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY
zcl identify query
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE
zcl identify ez-mode [action:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER
zcl identify trigger [effectId:1] [effectVariant:1]

Detailed Description

This group describes the CLI commands for the Identify cluster. Listed below is a description of the cluster:

Attributes and commands for putting a device into Identification mode (e.g. flashing a light).

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE

zcl identify ez-mode [action:1]

  • Invoke EZMode on an Identify Server
    • action - BITMAP8

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID

zcl identify id [identifyTime:2]

  • Command description for Identify
    • identifyTime - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY

zcl identify query

  • Command description for IdentifyQuery

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER

zcl identify trigger [effectId:1] [effectVariant:1]

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF

zcl identify off [endpoint:1]

  • Writes the IdentifyTime attribute
    • endpoint - INT8U - The endpoint on which to stop identifying

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON

zcl identify on [endpoint:1] [time:2]

  • Writes the IdentifyTime attribute
    • endpoint - INT8U - The endpoint on the device which should begin identifying
    • time - INT16U - The number of seconds to spend identifying