EmberAfRemoteBindingStruct Struct Reference
Zigbee Internet Client/Server Remote Binding struct.
#include <
af-types.h
>
Data Fields |
|
| EmberEUI64 | targetEUI64 |
| uint8_t | sourceEndpoint |
| uint8_t | destEndpoint |
| uint16_t | clusterId |
| EmberEUI64 | destEUI64 |
| EmberEUI64 | sourceEUI64 |
Zigbee Internet Client/Server Remote Binding struct.
Field Documentation
◆ clusterId
| uint16_t EmberAfRemoteBindingStruct::clusterId |
◆ destEndpoint
| uint8_t EmberAfRemoteBindingStruct::destEndpoint |
◆ destEUI64
| EmberEUI64 EmberAfRemoteBindingStruct::destEUI64 |
◆ sourceEndpoint
| uint8_t EmberAfRemoteBindingStruct::sourceEndpoint |
◆ sourceEUI64
| EmberEUI64 EmberAfRemoteBindingStruct::sourceEUI64 |
◆ targetEUI64
| EmberEUI64 EmberAfRemoteBindingStruct::targetEUI64 |
The documentation for this struct was generated from the following file:
-
af-types.h