Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST
plugin ota-client block-test
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD
plugin ota-client bootload [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_DISABLE_DOWNGRADES
plugin ota-client disable-downgrades
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_ENABLE_DOWNGRADES
plugin ota-client enable-downgrades
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO
plugin ota-client info
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST
plugin ota-client page-request [pageRequest:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT
plugin ota-client pause-at [stopDownloadPercentage:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START
plugin ota-client start
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS
plugin ota-client status
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP
plugin ota-client stop
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST
plugin ota-client upgrade-request
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY
plugin ota-client verify [index:1]

Detailed Description

The OTA Client plugin provides Over-the-air commands for upgrading firmware and downloading specific files on the client side.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST

plugin ota-client block-test

  • Sends an image block request for a file the server should not have. Test harness only (test case 9.5.6 - Missing File)

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD

plugin ota-client bootload [index:1]

  • Bootloads the image at the specified index by calling the OTA bootload callback.
    • index - INT8U - The index at which to begin bootloading the image

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_DISABLE_DOWNGRADES

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_DISABLE_DOWNGRADES

plugin ota-client disable-downgrades

  • Disable OTA downgrades

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_ENABLE_DOWNGRADES

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_ENABLE_DOWNGRADES

plugin ota-client enable-downgrades

  • Enable OTA downgrades

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO

plugin ota-client info

  • Prints the manufacturer ID, Image Type ID, and Version information that are used when a query next image is sent to the server by the client

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST

plugin ota-client page-request [pageRequest:1]

    • pageRequest - INT8U - boolean value turning on (1) or off (0) the page request flag

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT

plugin ota-client pause-at [stopDownloadPercentage:1]

    • stopDownloadPercentage - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START

plugin ota-client start

  • Starts the ota client state machine. The state machine discovers the OTA server, queries for new images, downloads the images and waits for the server command to upgrade

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS

plugin ota-client status

  • Prints information on the current state of the OTA client download.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP

plugin ota-client stop

  • Stops the OTA state machine

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST

plugin ota-client upgrade-request

  • Send an OTA server an UpgradeEndRequest

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY

plugin ota-client verify [index:1]

  • Perform signature verification on the image at the specified index
    • index - INT8U - The index at which to begin verification of the image