Detailed Description
The Network command set provides commands for interacting with the network. This includes building as well as sending ZigBee commands out on to the network.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_BROAD_PJOIN |
network broad-pjoin [seconds:1]
- Permit joining on the network for a given number of seconds AND broadcast a ZDO Mgmt Permit Joining request to all routers.
- seconds - INT8U - Number of seconds during which devices will be allowed to join the network. A value of 0xff turns permit joining on permanently
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_CHANNEL |
network change-channel [channel:1]
- Attempts to change device over to a different channel given in the channel argument.
- channel - INT8U - The channel to change to.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_EXTPANID |
network extpanid [extPanId:-1]
- Write the extended pan id for the device.
- extPanId - OCTET_STRING - The bytes for the extended pan id
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_JOINABLE |
network find joinable
- Begin a search for a joinable network. Will automatically attempt to join the first network that it finds.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_UNUSED |
network find unused
- Begin a search for an unused Channel and Pan Id. Will automatically form a network on the first unused Channel and Pan Id it finds.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FORM |
network form [channel:1] [power:1] [panId:2]
- Create a network on the given channel, power and panId.
- channel - INT8U - The channel on which to form the network
- power - INT8S - One byte signed value indicating the TX power that the radio should be set to
- panId - INT16U - Two byte pan id for the network
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ID |
network id
- Prints the current Node ID, EUI64, and Pan ID.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_INIT |
network init
- Initialize a network; this is a test command used for tc-swap-out testing.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_JOIN |
network join [channel:1] [power:1] [panId:2]
- Join an existing network on the given channel, power and panId.
- channel - INT8U - The channel on which to form the network
- power - INT8S - One byte signed value indicating the TX power that the radio should be set to
- panId - INT16U - Two byte pan id for the network
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_LEAVE |
network leave
- Leave the current network.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_START |
network multi-phy-start [page:1] [channel:1] [power:1]
- To start multi phy interface other than native and form the network. The stack uses same PanId as native radio network.
- page - INT8U - The page on which to form the network.
- channel - INT8U - The channel on which to form the network.
- power - INT8S - One byte signed value indicating the TX power that the radio should be set to
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_STOP |
network multi-phy-stop
- Terminates the multi phy interface
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_PJOIN |
network pjoin [seconds:1]
- Permit joining on the network for a given number of seconds
- seconds - INT8U - Number of seconds during which devices will be allowed to join the network. A value of 0xff turns permit joining on permanently
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN |
network rejoin [haveCurrentNetworkKey:1] [channelMask:4]
- Rejoin an existing network in a secure or insecure manner.
- haveCurrentNetworkKey - INT8U - Boolean indicating whether the device can rejoin secure or not. 1=rejoin with encryption, 0=rejoin without encryption
- channelMask - INT32U - 4 byte channel mask which should be used to search for the network to rejoin.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN_DIFF_DEVICE_TYPE |
network rejoin-diff-device-type [haveCurrentNetworkKey:1] [channelMask:4] [nodeType:1]
- Rejoin an existing network in a secure or insecure manner with a different device type.
- haveCurrentNetworkKey - INT8U - Boolean indicating whether the device can rejoin secure or not. 1=rejoin with encryption, 0=rejoin without encryption
- channelMask - INT32U - 4 byte channel mask which should be used to search for the network to rejoin.
- nodeType - INT8U - An enumeration indicating the device type to rejoin as.The stack only accepts EMBER_END_DEVICE and EMBER_SLEEPY_END_DEVICE.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_SET |
network set [networkIndex:1]
- Set the network index used by all future CLI commands. Before executing a CLI command, the framework will switch to this network. After the command finishes executing, the framework will switch back to the previous network. The CLI uses the same network index until the device resets or it is changed through this command.
- networkIndex - INT8U - The network index to use for CLI commands
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_DEFAULT |
option apsretry default
- Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; a value of "default" allows the AppFramework to use its own default logic to determine when the APS Retry option should be used.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_OFF |
option apsretry off
- Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; Turns APS retry off
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_ON |
option apsretry on
- Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; Turns APS retry on.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_CLEAR |
option binding-table clear
- Clear the binding table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_SET |
option binding-table set [bindingTableIndex:1] [clusterId:2] [localEndpoint:1] [remoteEndpoint:1] [ieeeAddress:8]
- Set a binding table entry for the arguments specified.
- bindingTableIndex - INT8U - one byte index into the binding table
- clusterId - INT16U - cluster id to send with the discovery message
- localEndpoint - INT8U - local endpoint to bind
- remoteEndpoint - INT8U - remote endpoint to bind
- ieeeAddress - IEEE_ADDRESS - 8 byte IEEE address provided big endian
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_DISC |
option disc [profileId:2] [clusterId:2]
- Sends a ZDO Match Descriptor Request for the server side of the specified cluster from the specified application profile. Match Descriptor Responses received are printed to the serial output.
- profileId - INT16U - the profile id to send with the discovery message
- clusterId - INT16U - cluster id to send with the discovery message
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_EDB |
option edb [endpoint:1]
- Sends a ZDO End Device Bind Request using the given local endpoint.
- endpoint - INT8U - The local endpoint whose simple descriptor will be used to create the request