Detailed Description
The Security command set includes all of the commands related to security configuration on the device.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI__SECURITY_MFG_TOKEN_COMMANDS |
Commands used for security.
security mfg-token get security mfg-token set <Magic number> <EmberKeySettings value>
- Magic number - uint32_t. The 4-byte magic number EMBER_MFG_SECURITY_CONFIG_MAGIC_NUMBER to prevent accidental execution.
- EmberKeySettings value - uint16_t. The 2-byte value for EmberKeySettings indicating key permissions.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_LINK |
changekey link [key:-1]
- Change the link key to the one provided in the 16 byte array argument for this command.
- key - OCTET_STRING - The link key provided as a 16 byte array
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_NETWORK |
changekey network [key:-1]
- Change the network key to the 16 byte array provided as an argument to this command.
- key - OCTET_STRING - The network key provided as a 16 byte array
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_CLEAR |
keys clear
- Clear all security keys
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_DELETE |
keys delete [index:1]
- Delete a security key from a given index
- index - INT8U - index into the security key table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_PRINT |
keys print
- Print all security keys out to the command line.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_INSTALL_CODE |
option install-code [keyTableIndex:1] [ieeeAddress:8] [installCode:-1]
- Derives a link key from an install code and sets it in the link key table.
- keyTableIndex - INT8U - index into the link key table
- ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
- installCode - OCTET_STRING - install code including two-byte, little-endian CRC
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_LINK |
option link [keyTableIndex:1] [ieeeAddress:8] [linkKey:-1]
- Sets a link key in the link key table. Example: option link 0x00 { 06 00 ab 41 64 30 00 0a } {aa bb cc dd ee ff aa bb cc dd ee ff aa bb cc dd}
- keyTableIndex - INT8U - index into the link key table
- ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
- linkKey - OCTET_STRING - link key to enter into the table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_REGISTER |
option register
- Initiates Smart Energy Registration including Key Establishment. This command expects that the device has already joined a smart energy network.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_OFF |
option security aps off
- Turns aps security off
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_ON |
option security aps on
- Turns aps security on
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY |
option security set-allow-trust-center-rejoin-using-well-known-key [allowTrustCenterRejoinUsingWellKnownKey:1]
- Set whether or not a Trust Center application will allow trust center rejoins for devices using the well-known key.
- allowTrustCenterRejoinUsingWellKnownKey - BOOLEAN - Whether or not the Trust Center should allow trust center rejoins for devices using the well-known key.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY_TIMEOUT |
option security set-allow-trust-center-rejoin-using-well-known-key-timeout [trustCenterRejoinUsingWellKnownKeyTimeout:2]
- Sets the number of seconds to allow trust center rejoins for devices using the well-known key. A value of 0 means the policy should not be changed after a timeout. This must be called prior to forming or joining a network.
- trustCenterRejoinUsingWellKnownKeyTimeout - INT16U - The number of seconds that trust center rejoins will be responded to using the well-known link key.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_KEY_REQUEST_POLICY |
option security set-key-request-policy [tcLinkKeyRequestPolicy:1] [appLinkKeyRequestPolicy:1]
- Sets the local policy for handling TC link key requests and application link key requests. This command sets the emberTrustCenterLinkKeyRequestPolicy and emberAppLinkKeyRequestPolicy attributes. This command should only be entered on the trust center.
- tcLinkKeyRequestPolicy - INT8U - The value to assign to emberTrustCenterLinkKeyRequestPolicy
- appLinkKeyRequestPolicy - INT8U - The value to assign to emberAppLinkKeyRequestPolicy
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_GET |
security mfg-token get
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_SET |
security mfg-token set [magicNumber:4] [value:2]
- magicNumber - INT32U
- value - INT16U