Plugin Commands: PS Store
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_DELETE_TAG |
plugin ps-store delete-tag [tag:2] [flags:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_DUMP |
plugin ps-store dump | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_INIT |
plugin ps-store init | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_PRINT_TAGS |
plugin ps-store print-tags | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_WRITE_TAG |
plugin ps-store write-tag [tag:2] [flags:1] [len:1] [val:-1] |
Detailed Description
Commands for the PS Store plugin, which manages data in flash memory.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_DELETE_TAG |
plugin ps-store delete-tag [tag:2] [flags:2]
- Writes tag to storage module.
- tag - INT16U - The tag or key.
- flags - INT16U - The mask to apply to the tag or key. 0 deletes all keys.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_DUMP |
plugin ps-store dump
- Prints the contents in the entire storage module.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_INIT |
plugin ps-store init
- Initializes the storage module.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_PRINT_TAGS |
plugin ps-store print-tags
- Prints all tags (or keys) in the storage module.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PSSTORE_PLUGIN_PS_STORE_WRITE_TAG |
plugin ps-store write-tag [tag:2] [flags:1] [len:1] [val:-1]
- Writes tag to storage module.
- tag - INT16U - The tag or key.
- flags - INT8U - The flags that apply to this record.
- len - INT8U - The length of the data to write.
- val - OCTET_STRING - The data values to write.