Functions

void emberAfPluginTransportMqttStateChangedCallback (EmberAfPluginTransportMqttState state)
 MQTT client state is changed.
 
bool emberAfPluginTransportMqttMessageArrivedCallback (const char *topic, const char *payload)
 MQTT message arrived.

Detailed Description

These callbacks are contributed by the Gateway MQTT Transport plugin.

Function Documentation

bool emberAfPluginTransportMqttMessageArrivedCallback ( const char *  topic,
const char *  payload 
)

MQTT message arrived.

This function is called when the MQTT client for the gateway receives an incoming message on a topic. If the message is processed by the application, return true. If the message is not processed, return false. This function is called on a separate thread, so no stack calls should be made within the implementation of this function. Instead, use a global variable in that function to communicate the message arrival to a stack event or timer running from the main loop.

Parameters
topicA string containing the topic for the message that arrived. While the underlying MQTT libraries allow NULL characters in a topic, NULL characters are not supported in this implementation so the topic parameter can be assumed to be NULL terminated.
payloadA string containing the payload for the message that arrived.
void emberAfPluginTransportMqttStateChangedCallback ( EmberAfPluginTransportMqttState  state)

MQTT client state is changed.

This function is called when the state of the MQTT client changes.

Parameters
stateContains the new and current EmberAfPluginTransportMqttState state.