Plugin Commands: BLE
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_CONNECTION_CLOSE |
plugin ble connection close [connection-handle:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_CONN_OPEN |
plugin ble gap conn-open [address:-1] [address-type:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_DISCOVER |
plugin ble gap discover [discovery-mode:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_ADV_PARAMS |
plugin ble gap set-adv-params [min-interval:2] [max-interval:2] [channel-map:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_BT5_MODE |
plugin ble gap set-bt5-mode [advertisement-handle:1] [discoverable-mode:1] [connectable-mode:1] [max-events:2] [address-type:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_CONN_PARAMS |
plugin ble gap set-conn-params [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_MODE |
plugin ble gap set-mode [discoverable-mode:1] [connectable-mode:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_UPDATE_CONN_PARAMS |
plugin ble gap update-conn-params [connection-handle:2] [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_CHARACTERISTICS |
plugin ble gatt discover-characteristics [connection-handle:1] [serice-handle:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_PRIMARY_SERVICES |
plugin ble gatt discover-primary-services [connection-handle:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_SET_CHARACTERISTIC_NOTIFICATION |
plugin ble gatt set-characteristic-notification [connection-handle:1] [characteristic-handle:2] [flags:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_WRITE_CHARACTERISTIC |
plugin ble gatt write-characteristic [connection-handle:1] [characteristic-handle:2] [value-len:1] [value-data:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GET_ADDRESS |
plugin ble get address | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_HELLO |
plugin ble hello | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_ALL_BONDINGS |
plugin ble sm delete-all-bondings | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_BONDING |
plugin ble sm delete-bonding [boning-handle:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_INCREASE_SECURITY |
plugin ble sm increase-security [connection-handle:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_LIST_ALL_BONDINGS |
plugin ble sm list-all-bondings | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_SET_BONDABLE_MODE |
plugin ble sm set-bondable-mode [bondable-mode:1] |
Detailed Description
The BLE plugin contributes CLI commands to the application framework to be used for initiating actions at the BLE stack.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_CONNECTION_CLOSE |
plugin ble connection close [connection-handle:1]
- Close BLE connection
- connection-handle - INT8U - the connection handle which should be closed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_CONN_OPEN |
plugin ble gap conn-open [address:-1] [address-type:1]
- Open a GAP connection
- address - OCTET_STRING - The BLE address of the target device
- address-type - INT8U - The address type: 0=public, 1=random, 2=public resolved by the stack, 3=public resolved by the stack, 16=classic bluetooth
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_DISCOVER |
plugin ble gap discover [discovery-mode:1]
- Start a GAP discovery procedure
- discovery-mode - INT8U - The GAP discovery mode: 0=only limited discoverable devices, 1=limited and generic discoverable devices, 2=all devices
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_ADV_PARAMS |
plugin ble gap set-adv-params [min-interval:2] [max-interval:2] [channel-map:1]
- Set the GAP advertisement parameters
- min-interval - INT16U - minimum connection interval
- max-interval - INT16U - maximum connection interval
- channel-map - INT8U - Channel map indicating which of three channels will be used
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_BT5_MODE |
plugin ble gap set-bt5-mode [advertisement-handle:1] [discoverable-mode:1] [connectable-mode:1] [max-events:2] [address-type:1]
- Set the BT5 GAP mode
- advertisement-handle - INT8U - The handle index of advertisement
- discoverable-mode - INT8U - The GAP discoverable mode: 0=non discoverable, 1=limited discoverable, 2=general discoverable, 3=broadcast, 4=user data
- connectable-mode - INT8U - The GAP connectable mode: 0=non connectable, 1=directed connectable, 2=undirected connectable, 3=scannable non connectable
- max-events - INT16U - The maximum number of events
- address-type - INT8U - Address type: 0=public, 1=random, 2=public identity, 3=random identity, 16=classic bluetooth
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_CONN_PARAMS |
plugin ble gap set-conn-params [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]
- Set the GAP connection parameters
- min-interval - INT16U - minimum connection event interval
- max-interval - INT16U - maximum connection event interval
- slave-latency - INT16U - number of connection intervals the slave can skip
- supervision-timeout - INT16U - time before the connection is dropped
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_MODE |
plugin ble gap set-mode [discoverable-mode:1] [connectable-mode:1]
- Set the GAP mode
- discoverable-mode - INT8U - The GAP discoverable mode: 0=non discoverable, 1=limited discoverable, 2=general discoverable, 3=broadcast, 4=user data
- connectable-mode - INT8U - The GAP connectable mode: 0=non connectable, 1=directed connectable, 2=undirected connectable, 3=scannable non connectable
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_UPDATE_CONN_PARAMS |
plugin ble gap update-conn-params [connection-handle:2] [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]
- Set the GAP connection parameters for connection
- connection-handle - INT16U - connection handle
- min-interval - INT16U - minimum connection event interval
- max-interval - INT16U - maximum connection event interval
- slave-latency - INT16U - number of connection intervals the slave can skip
- supervision-timeout - INT16U - time before the connection is dropped
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_CHARACTERISTICS |
plugin ble gatt discover-characteristics [connection-handle:1] [serice-handle:4]
- GATT discovery of characteristics
- connection-handle - INT8U - the connection handle on which discovery should be performed
- serice-handle - INT32U - the service handle on which discovery should be performed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_PRIMARY_SERVICES |
plugin ble gatt discover-primary-services [connection-handle:1]
- GATT discovery of primary services
- connection-handle - INT8U - the connection handle on which discovery should be performed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_SET_CHARACTERISTIC_NOTIFICATION |
plugin ble gatt set-characteristic-notification [connection-handle:1] [characteristic-handle:2] [flags:1]
- GATT set characteristic notification
- connection-handle - INT8U - the connection handle for which the notification should be set
- characteristic-handle - INT16U - the characteristic handle to set notification for
- flags - INT8U - 0=disable, 1=notification, 2=indication
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_WRITE_CHARACTERISTIC |
plugin ble gatt write-characteristic [connection-handle:1] [characteristic-handle:2] [value-len:1] [value-data:-1]
- GATT write characteristic value
- connection-handle - INT8U - the connection handle
- characteristic-handle - INT16U - the characteristic handle
- value-len - INT8U - the lenght of data
- value-data - OCTET_STRING - data to write
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GET_ADDRESS |
plugin ble get address
- Read the Bluetooth address
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_HELLO |
plugin ble hello
- Can be used to check that Bluetooth stack is functional
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_ALL_BONDINGS |
plugin ble sm delete-all-bondings
- Delete all bondings
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_BONDING |
plugin ble sm delete-bonding [boning-handle:1]
- Delete bonding
- boning-handle - INT8U - the bonding handle to be deleted
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_INCREASE_SECURITY |
plugin ble sm increase-security [connection-handle:1]
- Increase the security level
- connection-handle - INT8U - the connection handle for which we want to increase the security level
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_LIST_ALL_BONDINGS |
plugin ble sm list-all-bondings
- Send a command to get all the current bondings
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_SET_BONDABLE_MODE |
plugin ble sm set-bondable-mode [bondable-mode:1]
- Set the bondable mode
- bondable-mode - INT8U - The bondable mode: 0=new bondings not accepted, 1=bondings allowed