EmberAfCommandMetadata Struct Reference
A data struct used to keep track of incoming and outgoing commands for command discovery.
#include <
af-types.h
>
Data Fields | |
uint16_t | clusterId |
uint8_t | commandId |
uint8_t | mask |
A data struct used to keep track of incoming and outgoing commands for command discovery.
Field Documentation
uint16_t EmberAfCommandMetadata::clusterId |
uint8_t EmberAfCommandMetadata::commandId |
uint8_t EmberAfCommandMetadata::mask |
The documentation for this struct was generated from the following file:
af-types.h