Plugin Commands: Interpan
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_DISABLE |
plugin interpan disable | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_ENABLE |
plugin interpan enable | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_FRAGMENT_TEST |
plugin interpan fragment-test [panId:2] [eui64:8] [clusterId:2] [msgLen:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_SET_MSG_TIMEOUT |
plugin interpan set-msg-timeout [timeout:1] |
Detailed Description
The Interpan commands provide commands to set global interpan state and test interpan fragmentation.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_DISABLE |
plugin interpan disable
- Disables inter-PAN globally.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_ENABLE |
plugin interpan enable
- Enables inter-PAN globally.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_FRAGMENT_TEST |
plugin interpan fragment-test [panId:2] [eui64:8] [clusterId:2] [msgLen:2]
- Sends a message of specified length of random values to target device over inter-PAN.
- panId - INT16U - The PAN ID that the target is located on
- eui64 - IEEE_ADDRESS - The target's EUI64 (big endian)
- clusterId - INT16U - The cluster ID that the sample message should contain
- msgLen - INT16U - The length of the randomly-filled message to be sent across inter-PAN
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_SET_MSG_TIMEOUT |
plugin interpan set-msg-timeout [timeout:1]
- Sets the timeout for inter-PAN messages sent and received.
- timeout - INT8U - Message timeout in seconds.