EmberAfRemoteBindingStruct Struct Reference
Zigbee Internet Client/Server Remote Binding struct.
#include <
af-types.h
>
Data Fields | |
EmberEUI64 | targetEUI64 |
uint8_t | sourceEndpoint |
uint8_t | destEndpoint |
uint16_t | clusterId |
EmberEUI64 | destEUI64 |
EmberEUI64 | sourceEUI64 |
Zigbee Internet Client/Server Remote Binding struct.
Field Documentation
uint16_t EmberAfRemoteBindingStruct::clusterId |
uint8_t EmberAfRemoteBindingStruct::destEndpoint |
EmberEUI64 EmberAfRemoteBindingStruct::destEUI64 |
uint8_t EmberAfRemoteBindingStruct::sourceEndpoint |
EmberEUI64 EmberAfRemoteBindingStruct::sourceEUI64 |
EmberEUI64 EmberAfRemoteBindingStruct::targetEUI64 |
The documentation for this struct was generated from the following file:
af-types.h