stack API Callbacks
Functions | |
void | emberCounterHandler (EmberCounterType type, EmberCounterInfo info) |
Invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack. | |
bool | emberRtosIdleHandler (uint32_t *idleTimeMs) |
Allows the application to manage idling the MCU. | |
void | emberRtosStackWakeupIsrHandler (void) |
Requests the application to wake up the stack task. | |
void | emberStackStatusHandler (EmberStatus status) |
Invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the ::emberGetNetworkParameters() function can be called to obtain the new network parameters. If any of the parameters are being stored in nonvolatile memory by the application, the stored values should be updated. | |
void | emberEnergyScanResultHandler (uint8_t channel, int8_t maxRssiValue) |
Reports the maximum RSSI value measured on the channel. | |
void | emberRadioNeedsCalibratingHandler (void) |
The radio calibration callback function. |
Detailed Description
These callbacks were contributed by the stack API.
Function Documentation
void emberCounterHandler | ( | EmberCounterType | type, |
EmberCounterInfo | info |
||
) |
Invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
The application must define ::EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
- Parameters
-
type
The type of the event. info
could map to: - data: For transmission events, the number of retries used. For most other events, this parameter is unused and is set to zero.
- phyIndex: use for mac specific counters specifying if they belong to SubGhz or 2.4
- destinationNodeId: identifying which connection/destinationId a specific counter refers to
- Any combination of parameters above
void emberEnergyScanResultHandler | ( | uint8_t | channel, |
int8_t | maxRssiValue |
||
) |
Reports the maximum RSSI value measured on the channel.
- Parameters
-
channel
The 802.15.4 channel number on which the RSSI value was measured. maxRssiValue
The maximum RSSI value measured (in units of dBm).
void emberRadioNeedsCalibratingHandler | ( | void |
| ) |
The radio calibration callback function.
The Voltage Controlled Oscillator (VCO) can drift with temperature changes. During every call to ::emberTick(), the stack will check to see if the VCO has drifted. If the VCO has drifted, the stack will call emberRadioNeedsCalibratingHandler() to inform the application that it should perform calibration of the current channel as soon as possible. Calibration can take up to 150 ms. The default callback function implementation provided here performs calibration immediately. The application can define its own callback by defining ::EMBER_APPLICATION_HAS_CUSTOM_RADIO_CALIBRATION_CALLBACK in its CONFIGURATION_HEADER. It can then failsafe any critical processes or peripherals before calling ::emberCalibrateCurrentChannel(). The application must call ::emberCalibrateCurrentChannel() in response to this callback to maintain expected radio performance.
bool emberRtosIdleHandler | ( | uint32_t * | idleTimeMs | ) |
Allows the application to manage idling the MCU.
- Returns
- True if the application is managing idling the MCU, false otherwise. If this function returns false, the stack will manage idling the MCU.
void emberRtosStackWakeupIsrHandler | ( | void |
| ) |
Requests the application to wake up the stack task.
void emberStackStatusHandler | ( | EmberStatus | status | ) |
Invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the ::emberGetNetworkParameters() function can be called to obtain the new network parameters. If any of the parameters are being stored in nonvolatile memory by the application, the stored values should be updated.
The application is free to begin messaging once it receives the EMBER_NETWORK_UP status. However, routes discovered immediately after the stack comes up may be suboptimal. This is because the routes are based on the neighbor table's information about two-way links with neighboring nodes, which is obtained from periodic Zigbee Link Status messages. It can take two or three link status exchange periods (of 16 seconds each) before the neighbor table has a good estimate of link quality to neighboring nodes. Therefore, the application may improve the quality of initially discovered routes by waiting after startup to give the neighbor table time to be populated.
- Parameters